Blog - Events
0 of 0 votes

ON Semiconductor to Demo Mobile Communications and Connectivity Technologies at Mobile World Congress
by Kris Costers - 2018-02-22 09:32:23.0

ON Semiconductor will be hosting a series of demos relating to its latest semiconductor technologies for mobile communications and connectivity at Mobile World Congress. The company’s presence aligns closely with some of the core themes of the show which include the 4th Industrial Revolution (Industry 4.0) and Tech in Society.

Held in two meeting rooms on the 24th floor of the Porta Fira Hotel situated next to the Fira Gran Via, ON Semiconductor’s intuitive demonstrations will showcase the latest solutions for areas including:

Qi EPP Wireless Power TX-RX System Solution,

The receiver, NCP6400, is a Qi compliant wireless power receiver for applications up to 15W of power. Its flexible design integrates a high efficiency synchronous rectifier converting the AC power signal into DC voltage and the very popular 32-bit ARM Cortex M0+ processor. The DC output power is delivered through a programmable power switch with pass-through mode or low dropout voltage regulation. The device is a powerful SoC design offering system engineers the option to implement various wireless charging standards. The transmitter, NCV6500, is Qi EPP certified and includes local supply generation, full NMOS H-bridge drivers, on-chip clock generation with phase shifting and duty cycle control, demodulation detectors and protection circuitry. The device can drive four coils with two adjacent coils at the same time achieving uniform flux distribution. NCV6500 is automotive qualified.

Smart Passive Sensor Turnkey Solution

ON Semiconductor’s smart passive sensor (SPS) solution is a wireless passive sensors, enabling remote sensing, data aggregation, analysis of temperature, moisture, proximity, and pressure. The smart passive sensor (SPS) turnkey system solution incorporates all the required hardware and software into a single kit which composed of sensor tags, reader, antenna and analytic software. By providing all required components as a turnkey kit, a user can simply plug in to measure, aggregate and analyze the data for various IoT applications including but not limited to smart agriculture and vehicle production.

High Power USB Type-C Superspeed Hub

ON Semiconductor’s latest USB reference design is far more than a hub.  It showcases ON Semiconductor’s latest automotive grade high efficiency USB Type-C power solutions delivering up to 100W per USB Type-C port.  This full automotive USB-PD solution allows you to quickly plug and play a wide range of loads and power levels.  The hub also incorporates our advanced USB SuperSpeed ESD protection, and re-driver technologies.  The demo shows how ON Semiconductor’s SuperSpeed solutions can increase performance, save development time and reduce BOM cost.

The company will also feature the latest releases and enhancements to its 2017 Internet of Things Development Kit (IDK) that supports the rapid and easy development and implementation of IoT applications. The IDK recently won the 2017 IoT Evolution Product of the Year Award from IoT Evolution magazine and IoT Evolution World, the leading magazine and website covering Internet-of-Things (IoT) technologies.

Please join ON Semiconductor at Mobile World Congress, the world’s largest gathering for the mobile industry. 

ON Semiconductor meeting rooms: Room Marina (with demos) and Room Llobregat on the 24th floor of hotel Porta Fira, right next to Fira Gran Via.

Post a Comment

Your email address will not be published. Required fields are marked *

Name*

Email*

Comment

Rating of Post

Cancel

Rating of comment

ON Semiconductor Full Web Site